Case Study

Bristol City Council turns to Confirm to streamline flood defense inspection data

An asset management solution capturing flood risk condition data on-site automates scoring and creates one source of truth

Bristol UK

Bristol City Council

Bristol City Council is a Lead Local Flood Authority serving a population of 472,500 across 34 wards, covering 110 sq. km. in one of the UK’s most populous cities.

Brightly Software was acquired by Siemens. All products and services are now offered under the Siemens Asset Management portfolio.

https://www.bristol.gov.uk/ 

Headquarters
Bristol City, England, UK
Products
Industry Sector
Government
Infrastructure
We’re saving a huge amount of time and can have much more confidence in the accuracy of the records we’re keeping.
Jenna Angle
Flood Risk Officer, Bristol City Council

Background 

It is important for Lead Local Flood Authorities (LLFAs) to understand what flood risk assets are located within their geographical area of responsibility and for their condition to be monitored over time. This is essential, not only as it is a statutory requirement under the Flood and Water Management Act for all LLFAs to maintain a register of all their flood risk assets, but also because it facilitates effective management of flood risk assets.  

Asset condition monitoring means necessary repairs can be made to assets in a timely manner before asset failure occurs. Asset failures can present an unnecessary and unexpected increase in flood risk to the surrounding area. 

The challenge 

Bristol City Council (BCC) LLFA is a long-term user of the Confirm asset management software solution, with all its flood risk assets on the Confirm asset management system. However, the associated asset condition data was not held on the system. There also was no method for this data to be directly input into the system whilst on-site assessing asset condition.  

BCC was hand-recording asset condition data and then transposing this information onto Excel spreadsheets to calculate and record overall asset condition scores. They used a standard, but complex, Environment Agency (T98) scoring process. 

This system therefore involved double handling of data, allowing ample opportunity for human error. It was an inefficient use of time and meant asset condition scores had to be individually calculated each time, for each asset.  

Site photos of assets were taken on smartphones and then had to be manually transferred across to relevant files held on the council’s own servers, segregated from the asset register. This was a time-consuming process. Having to double handle data also meant that there was not a single source of truth for all asset information. Photos were stored in files, condition information was stored in Excel spreadsheets and only general asset information was stored on Confirm. 

The solution 

Seeking a more efficient way of managing the entire process, BCC turned to Brightly — which was later acquired by Siemens — to see if there was a way for the Confirm system to manage it all. 

“The team were able to assist us in devising a way for the data to be input directly into Confirm,” says BCC Flood Risk Officer Jenna Angle. “Brightly technicians [now a part of Siemens] were able to write code which allowed the system to automatically calculate an overall condition score for each asset, based on more granular condition data for each asset element input by officers on site. They were also able to advise on functionality and system requirements.” 

The results 

The entire procedure has now been revolutionized. “There’s no longer any double handling of data,” Angle continues. “We’re able to input it straight into the user interface on ConfirmConnect via a tablet whilst on site, which is far more efficient than our previous process of recording on paper and then later transposing to digital records. We also no longer need to do time-consuming calculations to determine overall asset condition scores — as this is now done automatically when the user inputs the breakdown condition scores of asset elements — to then get an overall asset condition score. 

“We’re also able to review changes to asset conditions over time, as Confirm allows the storing of records over long periods without overwriting the previous record against the asset. The use of ConfirmConnect means we can also now upload asset pictures in real time while on site, and these are uploaded directly to the asset record in Confirm. Overall, we’re saving a huge amount of time and can have much more confidence in the accuracy of the records we’re keeping with Confirm as central source of information for all assets.” 

Nick Vague, Senior Consultant at Brightly (a part of Siemens) adds, “Bristol City Council has been gradually migrating more and more of its assets to Confirm over the years. When they came to us with the challenge of recording flood risk data, we were determined to find a way to process and store that information within the Confirm system for them as well. Asset management software is never a one-size-fits-all — there’s always a degree of bespoke adaptation required. We were delighted to be able to work with BCC to find a solution that’s improving accuracy and freeing up huge amounts of staff time to devote to other priorities.”

We also no longer need to do time-consuming calculations to determine overall asset condition scores.
Jenna Angle
Flood Risk Officer, Bristol City Council

Get quarterly insights