Case Study

New South Wales Land and Housing Corporation (LAHC) embraces predictive maintenance

Powerful, real-time insights and predictive modeling deliver quality social housing

Asset management software case study

New South Wales Land and Housing Corporation

LAHC manages over 125,000 properties valued at AU$62 billion — the largest portfolio in Australia. In 2024, the organization merged with others into Homes NSW.

Brightly Software was acquired by Siemens. All products and services are now offered under the Siemens Asset Management portfolio. 

https://www.nsw.gov.au/departments-and-agencies/homes-nsw 

Headquarters
New South Wales, AUS
Products
Industry Sector
Government
LAHC needed to be able to better visualize and make sense of the significant amount of data it captured. It also needed to draw insights from the data to predict future asset needs.

Background

As the demand for housing continues to outpace supply, those who can’t afford to house themselves can turn to NSW Land and Housing Corporation, one of the largest social housing providers in the southern hemisphere. LAHC provides safe short- and long-term rental housing for those in need. LAHC owns 125,000 properties, valued at around AU$62 billion — the largest property portfolio in Australia.

Property management falls into two groups:

  • 94,000 public housing residential dwellings directly managed by LAHC
  • 31,000 LAHC owned and managed by community housing providers

To manage its geographically extensive range of properties, LAHC divides its asset portfolio into three regions — North West, Western Sydney and South East — which are further divided into 15 areas to manage property maintenance. 

The challenge

The upkeep of such a large number of properties is considerable, with LAHC receiving over 600,000 work requests annually. To keep its properties in good condition and squeeze more out of every dollar, LAHC wanted to reduce reactive maintenance jobs — scheduling repairs when something breaks — to predictive or planned maintenance that resolves issues before they become problems.

To do this, LAHC needed to better visualize and make sense of the significant amount of data it captured, from the asset location, status and cost to its usage and current condition, as well as functional and compliance assessments. It also needed to draw insights from the data to predict future asset needs and develop realistic maintenance programs to help ensure dwellings are clean, safe and habitable in compliance with the Residential Tenancies Act.

The solution

To make evidence-based asset management decisions and plan maintenance work based on real-time insights and predictions, LAHC implemented Assetic asset register to help capture and visualize their data in one spot. For scenario modeling, it used Predictor to support short- and long-term investment decisions.

First, LAHC integrated numerous data sources into the Assetic asset register, including:

  • Property Assessment Surveys (PAS) on dwellings, buildings and common areas to store essential condition and defect data at a point in time
  • Detailed Property Assessment Surveys (DPAS), which cover sewers, stormwater, other building data and estate-related data
  • Historical data from the various surveys and inspections of each dwelling over time

PAS and DPAS asset data is stored at different levels of hierarchy in the Assetic asset register, and then dashboards are used to view the asset portfolios. DPAS are engineering inspections where they select around 25–35 complexes each calendar year. This helps them see how the condition is changing as it ages. LAHC staff assess the property condition data against historical maintenance data, allowing them to assess how quickly or slowly a property has aged or deteriorated.

LAHC uses the Predictor optimization model to guide its day-to-day work by understanding the outcome that different decisions would have — such as varying the investment, treatment or time the work is scheduled. It also uses Predictor to analyze its asset maintenance programs annually across its three regions, sharing the results with each area to help ensure all programs work as designed.

Evaluating how maintenance impacts the condition and functionality of property assets is essential in determining whether the program planning and delivery is well structured, resourced and managed. 

The results

LAHC has found that Predictor is a great tool for everyday work and strategic planning, as it presents data in easy-to-understand visuals to show stakeholders the long-term impact different funding decisions can have. Recently, they used Predictor to seek additional funding from the NSW Treasury. Not only were they awarded the funding, but they also won an honorable mention for the business case in the 2022 Premier’s Award.

Furthermore, LAHC uses the dashboard functionality to quickly and easily see all their property management and maintenance information. The asset hierarchy tree is especially handy as it can be seen at different levels — by the agency managing the property, by estate, or by asset component, asset ID, category and type. Even the property’s condition, such as the paint or windows, can be seen in the asset register. When an asset is selected in the hierarchy tree, it takes the user to the location of the asset on a map, which is especially useful when planning maintenance jobs.

Using data from the asset register, LAHC creates models in Predictor that enable it to assign different treatments for components at various intervention levels. LAHC knows that interior components are more important for tenant satisfaction and can pose greater safety risks if not maintained, so with Predictor, they can set intervention levels for interior repairs.

Predictor is also great for longer-term strategies such as 10-year planning. It is easy to ask questions of the data such as: What happens to the portfolio if LAHC does not receive any funding? If LAHC receives additional funding, where should that money be invested to have the greatest impact? What would be the split between reactive and planned maintenance at different funding levels? These questions help to understand what decisions will lead to the best outcome, both in terms of the portfolio conditions score and value for money.

LAHC now benchmark its properties based on different criteria, allowing it to see which properties are well maintained and which are not. They can easily see where excellent properties can be found and where they need to spend more money via a simple map visualization.  

As LAHC manages an increasing number of social housing properties, the asset management system is critical to their ability to deliver best value outcomes and maximize the ability of social housing properties to provide a safe and comfortable environment for more people in need in their communities. 

LAHC found that Predictor is a great tool for everyday work and strategic planning, as it presents data in easy-to-understand visuals to show stakeholders long-term impact.

Get quarterly insights