Case Study

The City of Salisbury’s digital transformation drives efficiency in field service processes

Confirm allows the city to manage jobs and inspections, respond to community requests and perform maintenance across its infrastructure operations

Asset management software case study

City of Salisbury

The City of Salisbury has a population of about 145,000 within 158 sq. km. (61 sq. mi.), with over 230,000 infrastructure assets at a replacement cost of $1.5 billion.

Brightly Software was acquired by Siemens. All products and services are now offered under the Siemens Asset Management portfolio.

https://www.salisbury.sa.gov.au/

Headquarters
Salisbury, South Australia, AUS
Products
Industry Sector
Government
Because of the near real-time tracking of status, jobs don’t fall through the cracks and our community see better outcomes.
James Corletto
Team Leader Strategic Asset Management, City of Salisbury

The challenge and opportunity

The City of Salisbury is a local government area located on the northern fringes of Adelaide, South Australia. It has a population of approximately 145,000 and encompasses an area of 158 km2. It manages over 230,000 infrastructure assets with a replacement cost of $1.5 billion.

The City of Salisbury has used technology as the cornerstone of its operations for decades and has achieved a high level of digital maturity. Part of its success was partnering with Brightly — later acquired by Siemens — to deploy an enterprise asset management system that interfaced with other major corporate systems, including its customer request management, finance system and geographic information system (GIS).

A major step on the city's journey was the digital transformation of field service processes that were heavily paper based. With 100 teams plus contractors working within the city to inspect and maintain a range of community infrastructure, it was essential they implemented a field solution that was flexible and easy to use. As a local public government, transparency is always a top consideration. Salisbury needed a solution that could track costs at a detailed level, enforce a range of safe working guidelines and improve operational efficiencies. 

From manual processes to digital transformation

The Council has historically operated with paper-based processes for activities conducted by its field services teams. With a broad range of activities and a need to capture increasingly detailed data, their manual processes had become too cumbersome and inefficient. With a goal to respond to community requests with an outcome within 10 days, leadership knew it was time to make the move to digital.

Salisbury established a project team to plan and execute this major transformation. It included the shift to using Confirm Connect to manage jobs and inspections, perform maintenance and respond to community requests across all infrastructure operations.

It also allows the Council to use dashboards to track the data for each asset, which includes everything from roads, play spaces, trees and reserve furniture. Every team member and manager can now see the status of all jobs, inspections and enquiries they are working on.

Additionally, using the Confirm Workzone solution, schedulers have a map-based view to drag-and-drop work to different teams. James Corletto, Team Leader Strategic Asset Management at the City of Salisbury says “when an urgent request comes in, coordinators simply look at the map that shows the location of all teams in real-time and then allocate the job to the closest team.”

“Because of the near real-time tracking of status, jobs don’t fall through the cracks and our community see better outcomes,” says Corletto. “If we aren’t able to complete an enquiry within the 10-day window, we can use the integration between Confirm and our Customer Request Management system to send the citizen a message with the status of their request.”

While in the field, employees use tablets to efficiently complete a range of asset-related tasks. Confirm offers a spatial view of assets and tasks which assists with asset identification. Each team completes a pre-start vehicle check and completes a job specific risk assessment prior to starting the work, eliminating the use of paper forms.  

Improving efficiency with Click and Collect

The City of Salisbury is now rolling out its Click and Collect program for materials and consumables, replacing their previous paper-based process.  

Salisbury identified that staff could eliminate multiple daily trips to the hardware store, freeing time for higher-value work. With the Click and Collect program, crews can collect a single box in the morning that contains the items they need.  

When teams complete their daily pre-start checklist in Confirm Connect they record if they are running low on materials and PPE items such as hardware, sunscreen and gloves. The data in Confirm is also used to prepare other materials that the team will need for the work they’ve been assigned. In addition to saving time looking for items, the process has significantly reduced delays because now employees have the right materials on hand and ready to go. 

Detailed labor and plant usage data is captured in Confirm Connect and transferred into the Council’s financial system to update all costs against the appropriate budget. Materials are then recorded against tasks to improve job cost reporting to cover labor, plant and materials. The new process reduces errors and provides stakeholders with an up-to-date picture of the budget. Managers can now more easily review budgets at monthly meetings and quickly know if they are overspending or underspending in specific areas.

Confirm Connect also makes working with contractors seamless. Previously, contractors used spreadsheets and email to track inspections and work, which created more work for Council employees and made it difficult to get an accurate picture of progress. Now Salisbury’s contractors can work directly in Confirm Connect. For example, the contractor that maintains drains can input their inspections which instantly updates a dashboard. Managers can see how many pits were cleaned and what inspections are still outstanding.

With a large number of infrastructure assets it is important that asset information is updated efficiently. Being able to complete updates in the corporate GIS and have them synchronize with Confirm means the spatial team can continue to use GIS technology they are familiar with and data is consistent across corporate systems. 

Looking to the future

As the City of Salisbury has increased its level of digital maturity, the jurisdiction has a much clearer picture of all costs in relation to service. With a single enterprise asset management system, a single view of every asset is possible — location, condition and maintenance history. As this valuable set of information no longer sits in spreadsheets or across unlinked systems, stakeholders now have a complete view and can make better informed decisions at both an operational and strategic level. 

When an urgent request comes in, coordinators simply look at the map that shows the location of all teams in real-time and then allocate the job to the closest team.
James Corletto
Team Leader Strategic Asset Management, City of Salisbury

Get quarterly insights