Blog

When should you replace an asset? Look beyond asset age

Key Takeaways 

  • Replacing assets based on age alone can overlook critical differences in performance and risk.
  • Operational intelligence provides the context needed to evaluate asset health and remaining value.
  • Connected asset data supports more effective lifecycle planning, capital allocation and infrastructure stewardship.

When to maintain, repair, upgrade or replace an asset is a near-daily consideration for many facilities teams. The answer is primarily guided by asset age, manufacturer life expectancy or periodic condition assessments — benchmarks that remain useful but only offer a partial view of the situation.

Two assets installed at the same time can perform differently depending on how they have been operated, maintained and utilized over the course of their service life. 

While replacement schedules are a good starting point, making sound asset lifecycle decisions requires a fuller operational context.

Operational intelligence uses real-time data to show how assets are performing and inform action. It brings asset, maintenance and operational data together, helping facilities teams evaluate assets within the context of how they are actually being used and maintained.

So, rather than viewing replacement as a calendar-driven event, facilities managers can make decisions based on how assets are actually performing in the environment they support.

Asset age isn’t enough

As helpful as asset age is to determine replacement windows, it cannot reveal whether an asset continues to operate reliably, how maintenance requirements have evolved over time or whether failure risk is increasing.

For example, two chillers of the same age may reach very different points in their lifecycle. One may remain reliable and cost-effective to maintain, while the other may show signs of declining performance, higher repair costs and greater failure risk. However, on paper they may appear equally due for replacement, leading to a one-size-fits-all approach that overlooks important operational differences.

Asset condition is shaped by numerous factors, including operational environment, maintenance history, utilization levels, reliability trends and operational criticality. Understanding these factors creates a more accurate assessment of asset health than age alone and helps facilities teams avoid both premature replacement and unnecessary risk.

Bringing asset and operational data together

Operational Intelligence provides the framework for connecting information that often exists in separate systems, records and repositories. It combines real-time asset data with maintenance histories, inspections, technical documentation and operational insights to provide a clearer understanding of asset performance and priorities. This connected view helps teams to identify:

  • Performance degradation that may develop gradually
  • Escalating maintenance costs Increasing failure risk 
  • Increasing failure risk
  • Remaining useful life
  • Opportunities to improve maintenance strategies

Operational intelligence preserves the relationships between data sources so maintenance work, condition information and operational requirements can be evaluated together. Those insights help facilities teams determine the most appropriate path forward.

For example, an asset with stable performance and manageable maintenance requirements may remain in service, while recurring repairs, escalating maintenance costs or increasing failure risk may indicate the need for corrective action.

In other cases, changing operational demands or performance limitations may support an upgrade, while declining reliability and rising costs may point toward replacement.

Better decisions, not simply longer asset life

 

A manufacturing technician interacting with a digital touchscreen interface on automated factory equipment, overlaid with a graphic green and white circle.

 

One of the most compelling outcomes associated with operational intelligence is the ability to extend equipment life. Siemens reports that organizations implementing real-time data strategies often achieve a 20% to 40% extension in useful asset life.

However, extending asset life should be viewed as a potential outcome, not the goal.

In some situations, connected asset data may reveal that an asset can continue operating safely and reliably for years beyond its expected replacement date. In others, the same information may show that a more immediate replacement is needed due to increasing risk, operating costs or performance concerns.

With operational intelligence providing the context, lifecycle decisions become less dependent on assumptions and more reflective of operational realities.

Connecting lifecycle decisions to capital planning

Maintenance teams often have a detailed understanding of which assets demand the most attention, generate the highest costs or create the greatest operational concerns. That knowledge does not always carry through to capital planning decisions.

Operational intelligence brings maintenance, operational and asset information into the broader planning process, creating a stronger basis for understanding where investment is needed and where existing assets can continue to deliver value. This supports:

  • More confident capital allocation decisions
  • Better infrastructure stewardship
  • Reduced replacement guesswork
  • Stronger risk management

Capital planning becomes less about asset age and replacement schedules and more about organizational priorities, operational requirements and the condition of the assets supporting them.

Make asset lifecycle decisions with confidence

Effective asset lifecycle management requires an in-depth understanding of how assets perform, how risk evolves and how maintenance workflows influence long-term outcomes.

Operational intelligence provides the context needed to bring those factors together, helping organizations make replacement decisions at the right time based on evidence rather than guesswork.

Learn how operational intelligence helps facilities teams turn real-time asset data into more informed maintenance and lifecycle decisions in our guide, Operational intelligence in asset management: A practical guide to using real-time data for better maintenance decisions.

Get insights from us

Get quarterly insights