Blog

Condition-based maintenance explained: Bridging the gap to predictive strategies

Key Takeaways

  • Real-time asset monitoring enables smarter maintenance decisions by using equipment performance data to identify issues early and schedule repairs only when needed.
  • Data-driven maintenance strategies reduce costs and improve reliability by minimizing unplanned downtime, extending asset life and optimizing labor and sparts usage.
  • Continuous asset health data supports advanced maintenance programs by providing insights needed to forecast failures, improve planning, and strengthen long-term operational performance.

For many facilities teams, preventive maintenance has been a welcome evolution, freeing them from the constant firefighting of 'fix it when it breaks' routines. This popular strategy utilizes scheduled inspections, routine servicing, and condition monitoring to detect early warning signs of asset failure.

However, even with its efficacy in preventing costly downtime, this form of asset maintenance has inherent limitations, including premature asset replacements, missed failures that fall outside servicing timelines, and the potential for reactive crises.

As organizations increasingly seek to evolve their maintenance strategies in the face of new digital transformation opportunities, the shift is towards proactive, data-driven management where asset health, not a clock, dictates decisions. This crucial leap to effective, reliable predictive maintenance, however, requires an indispensable incremental step: condition-based maintenance (CBM).

What is condition-based maintenance (CBM)?

Condition–based maintenance is the bridge to predictive maintenance that liberates facilities teams from rigid schedules by using real-time data to determine actual asset health. Relying on the continuous monitoring of an asset’s condition, CBM uses a variety of sensors and diagnostic tools to detect early signs of degradation, allowing maintenance to be performed only when needed, right before a potential failure occurs.

This dynamic asset health assessment provides an up-to-the-minute understanding of an asset’s actual condition to optimize maintenance schedules, minimize downtime, and extend the lifespan of equipment, moving beyond traditional time-based or reactive approaches. To achieve this, the continuous stream of information undergoes sophisticated processing and analysis that transforms raw data into actionable triggers that drive intelligent maintenance decisions.

Using raw sensor data — from vibrations and temperatures to pressure and acoustic emission — to derive actionable insights, CBM relies on three main decision points designed to flag potential issues long before they escalate into costly failures:

  1. Threshold Alerts: The most fundamental layer of CBM analysis involves setting pre-defined operational limits for various asset parameters. When a sensor reading exceeds or falls below these established thresholds, an immediate notification is triggered. For instance, if a motor's temperature suddenly spikes above its safe operating range, an alert is generated, signaling an anomaly that requires immediate attention. These alerts act as the first line of defense, catching sudden, critical deviations.
  2. Trend Analysis: Beyond simple thresholds, CBM excels at identifying subtle changes and evolving patterns in data that signal impending issues before they become critical. This is where CBM truly becomes proactive. Instead of waiting for a temperature to hit a critical limit, trend analysis might detect a gradual, consistent increase in temperature over several days, even if it's still within acceptable limits. This upward trend indicates a developing problem, allowing maintenance teams to proactively intervene during scheduled downtime, rather than reacting to an unexpected breakdown.
  3. Pattern Recognition: Advanced CBM systems leverage sophisticated algorithms, often including machine learning, to identify known failure signatures within the data. These failure indicators are learned from historical data of similar assets or known fault conditions. For example, a specific vibration frequency pattern might be recognized as indicative of a loose bolt, or a particular change in current draw might signal a winding insulation issue. By recognizing these patterns, CBM can pinpoint the nature of a developing fault with high accuracy, guiding maintenance personnel directly to the root cause.

Leveraging these three data-driven triggers, facilities teams gain the foresight to perform maintenance precisely when needed. This proactive predictive approach eliminates unnecessary interventions and catastrophic failures while also reducing labor costs, optimizing spart parts inventory, and minimizing waste.

Most critically, it maximizes component life by ensuring assets are utilized to their full operational potential. Instead of replacing parts on a fixed schedule or after a breakdown, CBM allows components to operate reliably for their entire useful life, extending asset longevity and maximizing the return on investment without compromising safety or performance.

CBM is an essential prerequisite for predictive maintenance

For organizations drafting digital transformation plans with predictive maintenance as the end goal, CBM is an essential prerequisite to truly achieve success. With condition monitoring as the fuel for predictive models, CBM provides:

  • Continuous, high-quality data that is the critical input for machine learning and AI algorithms used in predictive maintenance.
  • A rich history of asset behavior, degradation curves, and failure modes that are essential for training and validating predictive strategies.
  • A seamless transition from diagnosis to prognosis, enabling predictive models to forecast future failures and estimate an asset’s remaining useful life.

Ultimately, the integration of CBM data within predictive frameworks creates a powerful, continuous feedback loop. CBM systems constantly feed new operational data alongside the outcomes of maintenance actions back into the predictive models, allowing them to learn, adapt their algorithms, and improve their accuracy over time for optimal asset health.

The transformative benefits of CBM-driven workflows

CBM’s true value rests in the transformative benefits it brings to facilities teams, especially when shifting from reactive or time-based maintenance to data-driven strategies. This evolution allows organizations to unlock operational, financial, and efficiency advantages, including:

  • Elimination of Unplanned Downtime: By detecting potential failures before they happen, CBM allows for proactive, scheduled maintenance during planned downtime or low-impact periods, which reduces costly, disruptive breakdowns and scrambled delivery schedules.
  • Cost Optimization: CBM reduces overall maintenance costs by minimizing emergency repairs, optimizing spare parts inventory, and preventing secondary damage that is often the result of catastrophic failures.
  • Extended Asset Lifespan: Instead of replacing components based on arbitrary timeframes or after they’ve already failed, CBM allows for maintenance precisely when needed, effectively maximizing the asset’s useful life, bolstering capital planning, and improving return on investment (ROI).
  • Enhanced Safety and Compliance: CBM’s continuous monitoring helps detect anomalies that could lead to dangerous situations, enabling timely intervention and fostering a safer working environment. Consistent asset health also ensures compliance with operational standards and regulatory requirements.
  • Improved Operational Stability: With fewer unexpected breakdowns and optimized maintenance schedules, CBM paves the way for smoother, more predictable, and reliable operations.
  • Data-Driven Strategic Planning: The rich trove of data generated by CBM systems informs capital planning, asset lifecycle management (ALM) strategies, and future investment decisions. Understanding the true health and performance of assets allows organizations to make better choices about upgrades, replacements, and overall asset performance.

Practical steps for implementing CBM

Successful implementation of condition-based maintenance requires a structured approach that integrates technology, refines processes, and empowers teams.

It begins with strategic asset identification, which prioritizes critical assets, especially those whose failure would have the most impact on safety, production, quality, and costs. This first step ensures resources are allocated effectively and delivers the quickest ROI.

For the second step, teams must choose the right technology, including appropriate sensors (e.g., temperature, vibration, acoustic, current), data acquisition systems, and robust analytics platforms to process and interpret that data. These solutions should seamlessly integrate with existing enterprise systems, including ALM or enterprise asset management (EAM) platforms, to ensure a unified view of asset health and maintenance workflows.

Next, organizations should invest in workforce development by prioritizing personnel training in CBM system management, data interpretation, understanding alerts and trends, and adapting to new, proactive maintenance strategies, effectively moving facilities teams from reactive to proactive workflows.

Finally, to mitigate risks and ensure smooth adoption, organizations must take a phased approach to CBM implementation. Starting with pilot projects on a select number of critical assets, teams gain experience, refine processes, and demonstrate tangible benefits before scaling the CBM program across the entire organization.

The indispensable key to operational excellence

By leveraging real-time data to assess actual asset health, CBM is the fundamental paradigm shift that frees facilities teams from the constraints of fixed schedules and reactive cycles. This move toward more predictive strategies — fueled by high-quality data, historical context, and diagnostic capabilities — is the lynchpin in establishing intelligent, efficient, and sustainable operations.

To learn more about condition-based maintenance and better understand where you land on your digital transformation journey, download From Reactive to Predictive: A Guide to Next-Gen Asset Maintenance.

Get insights from us

Get quarterly insights