Press Release

NBOA: PPRRSM Wasn't Designed for Extreme Weather

Reading time: 5 minutes
Asset management software news

In the age of climate change, traditional calculations warrant new considerations.

The frequency of billion-dollar weather and climate disasters in the U.S. has increased from an average of three events per year in the 1980s to 20 events per year over the last decade. In 2025 alone, the U.S. experienced 23 such disasters. For facilities leaders at independent schools, the rise in weather and climate events translates directly into capital exposure.

When storm damage accelerates asset wear and emergency repairs compete with planned capital investments, the PPRRSM (Provision for Plant Replacement, Renewal and Special Maintenance) framework falls short. Designed to protect schools from funding shortfalls, PPRRSM was built for a steadier risk environment than what schools face today and without the asset-level data now required to manage it.

The actuarial assumptions that made PPRRSM reliable for decades break down when once-in-a-decade storms now arrive year after year. To keep reserve benchmarks aligned with actual capital risk, independent schools should revisit these assumptions and develop a more dynamic approach to long-term funding before the next storm forces the issue.

What PPRRSM Was Built For

Independent schools can't go to voters when a roof fails or a boiler gives mid-winter. And when disaster strikes, they are reluctant to apply for FEMA funds due to the Title IX requirements that come with accepting public funding. Instead, independent schools rely on PPRRSM as a capital reserve framework to set money aside before they need it. PPRRSM dictates schools contribute 3-5% of total plant replacement value annually, accumulating reserves against anticipated expenses.

Facilities leaders at independent schools can plan for asset failure and build replacement schedules around those timelines, funding them gradually. By its nature, PPRRSM doesn't account for unexpected events, but rather spreads costs over time, smoothing the financial impact of replacement cycles that would otherwise become emergencies.

The Impact of Climate Risk

A 2025 report from the Climate and Community Institute suggests that today's school building systems are "designed for a climate that doesn't exist." This suggests school's financial framework for building upkeep and replacement also warrants revisiting.

"Roughly 25% of public schools sit in census tracts facing high risk of at least one environmental hazard, including hurricanes, wildfires, flooding and hail."

According to the most recent NBOA data in BIIS, schools that have been consistently underfunding PPRRSM face a compounding problem, as deferred maintenance makes assets more vulnerable to weather damage, which accelerates the need for replacement, which deepens the backlog.

Roughly 25% of public schools sit in census tracts facing high risk of at least one environmental hazard, including hurricanes, wildfires, flooding and hail. While the data does not capture independent schools, they share the same geography and risk profile. What independent schools don't share is the recovery infrastructure.

The reserve that was supposed to fund a planned roof replacement in year 20 is now funding an emergency one in year 12. The gap between what PPRRSM assumes and the reality campuses face is growing faster than reserves.

Data Driven Change

Closing this gap requires shifting from assumption-based capital planning to decisions grounded in real-time asset data. PPRRSM's real value is in the discipline of setting aside reserves before capital needs arise. Independent school leaders should consider adding a climate risk layer to their PPRRSM frameworks. That starts with knowing a campus's assets well enough to distinguish between what's ageing and what's exposed. Accurate asset data is the precondition.

"With climate events stretching campus facilities budgets thinner, understanding what assets are at risk of failure versus what assets are scheduled to fail can mean the difference between strategic capital allocation and costly, reactive emergency spending."

A facilities condition assessment (FCA) establishes the baseline condition of every asset on campus, identifies what's aging, and surfaces what is already vulnerable to climate stress. For instance, an FCA would report damage to a school roof needing to be addressed before the next storm. Without an FCA, capital planning becomes an exercise in educated guessing. A campus can't right-size its PPRRSM reserves for climate risk if it's unclear which assets are one bad storm away from failure.

From there, a computerized maintenance management system (CMMS) can give facilities leaders the ability to prioritize capital based on real-time asset performance and risk. With climate events stretching campus facilities budgets thinner, understanding what assets are at risk of failure versus what assets are scheduled to fail can mean the difference between strategic capital allocation and costly, reactive emergency spending.

Using predictive maintenance schedules alone can lead to unnecessary replacements when asset data shows no signs of failure. With performance data is available, a facilities leader can defer that replacement and redirect capital toward an emergency reserve calibrated to today's risk environment. The goal isn't to abandon PPRRSM's discipline, but to make that discipline responsive to what the data is showing.

For independent schools, the path forward is not replacing PPRRSM but strengthening it with data. Schools that pair PPRRSM's long-standing financial discipline with real-time asset intelligence will be better positioned to protect reserves, prioritize investments and respond to climate risk without compromising long-term plans.

Author
Katie Gramajo Senior Education Specialist, Asset Management Software

Katie Gramajo serves as the Education Vertical Solutions Lead, at Asset Management Software by Siemens. Gramajo is an APPA Certified educational facilities professional with more than a decade of experience leading facilities operations, capital planning, sustainability initiatives, and campus logistics across independent K-12 schools.

Read the full article here.