Blog

Software integration explained: Your guide to understanding APIs and connected systems

Key takeaways

  • Software integration enables systems to share data and workflows, replacing siloed information with connected, end‑to‑end operational insight.
  • APIs provide a consistent way for applications to communicate, while integration platforms and patterns define the scalability, reliability and resilience of those connections.
  • Effective integration intentionally designs how systems connect, how data moves and how changes propagate, so operations remain scalable, reliable and aligned with real-world workflows.

Software integration is a crucial topic in today’s operational ecosystems. But let’s be honest: Discussions around it can often feel overwhelming, especially if you’re not from a technical background.

This guide is designed to demystify the basics of software integration, from understanding APIs to the different types of integrations and data exchange methods. Our goal is to equip you with the knowledge to confidently join any integration conversation and understand how connected systems can transform your organization.

What are software integrations?

Software integrations are the essential connections that allow different applications to talk and work together seamlessly. By linking processes and sharing data, rather than letting information sit in silos, everyone can do their jobs more effectively.

When data is no longer fragmented across systems, it supports reliable reporting and enables analytics and AI to operate on complete, trustworthy context. Properly integrated systems allow teams to spend less time questioning data and more time leveraging these shared, up-to-date views of operations into actionable insights.

The result is significant savings in time and money, fewer errors, less duplication and improved customer service.

For example, an asset manager seeking comprehensive data to guide decisions on building repairs and replacements can integrate maintenance data with capital planning software or Power BI to deliver the depth of insight needed.

Similarly, connecting maintenance planning with geographic information systems (GIS), scheduling and other productivity tools directly translates to more efficient daily repair workflows.

In asset management, the conversation inevitably turns to integrations, and understanding these connections is key to unlocking their full potential.

Six essential software integration terms

Before your next meeting, familiarize yourself with these six key integration terms to confidently join the conversation.

1. API: Application program interface

An API is a programmatic interface that allows software applications to communicate, exchange data and perform actions with each other. Think of it as a standardized touchscreen for your software, enabling seamless interaction.

For IT teams, APIs provide the definitions and protocols to integrate different programs. For users, APIs simplify access, allowing you to initiate tasks, create/update records and retrieve data just as if you were using the software directly.

A key advantage is automation: APIs make processes like data updates repeatable and efficient. Critically, an API's interface remains constant even as the underlying application undergoes upgrades, supporting consistent functionality.

2. REST API: Representational state transfer

REST is a popular, flexible architectural style for designing APIs. It uses simple functions (like GET, POST, PUT, DELETE) to exchange data over the HTTP protocol. Because REST APIs handle all data types across various devices and platforms, they are highly versatile. Their defined, unchanging fields help ensure your interface remains consistent, even with software updates. When you hear "REST API," it signifies a standard, consistent way for applications to communicate.

3. SOAP API: Simple object access protocol

SOAP is another protocol for building APIs, characterized by its strict standards and reliance on XML for message formatting. While often considered an older framework and less flexible than REST, SOAP APIs offer robust security and reliability. From a user's perspective, whether an API is REST or SOAP, both achieve the same goal of enabling application communication.

4. WSDL: Web service description language and Swagger (OpenAPI Specification)

These terms refer to API documentation. If someone mentions sending a "WSDL file," they're providing a definition of a SOAP web service's functionality. Similarly, a "Swagger doc" (now also known as OpenAPI Specification) describes how a REST API works. Both serve to document the API's capabilities for developers.

5. OData: Open Data Protocol

Developed by Microsoft, OData is a query protocol that provides a standardized, best-practice way to build and use REST APIs. It enforces a specific structure, using simple HTTP messages to allow users to publish and edit data. OData offers a uniform method to describe both the data and its underlying model. 

6. GraphQL

Created by Facebook, GraphQL is an API query language offering a more flexible and dynamic way to request data compared to REST APIs. It allows users to specify precisely what data they need (for example, specific details about assets and related work orders), receiving only that information. This precision can be highly efficient, though poorly formed queries can sometimes pose processing challenges for the service.

Using APIs for software integration

An API provides the interface for communication, but it doesn't automatically create a full integration. Think of an API as the connection point; you still need a dedicated integration platform to manage the actual flow of data and logic between applications. That orchestration is what allows data to move from collection, to context, to action — without manual intervention or lag.

These platforms, available both on-premise and in the cloud, are crucial for orchestrating seamless connections. As more organizations move to the cloud, cloud-based solutions like Microsoft Azure Logic, Power Automate, MuleSoft, Boomi and Amazon Web Services (AWS) offer powerful and flexible ways to link your systems.

In some cases, software vendors even provide their own integrated frameworks, streamlining the integration process directly within their applications.

Types of software integrations

Now that we’ve explored the building blocks of integration, let’s look at the different architectures or strategies you can use to connect software applications. Choosing the right approach depends on your organization’s needs, complexity and budget. While there’s no single right way, understanding these common types will help you decide what fits best:

  • Point-to-point: This directly integrates two systems, taking data out of one app and putting it into another. Point-to-point integrations are easy to implement because you know exactly what you’re dealing with. 
  • Hub and spoke (horizontal): Imagine a central command center, like an enterprise resource planning (ERP) system, acting as the hub. All other applications, the spokes, connect to this central hub. Data flows through this central point, providing a structured framework for integration. This approach supports a more continuous flow of information across systems, helping organizations maintain consistent asset histories and operational context over time. The main advantage is centralized control, but a drawback is that if the hub goes down, all connected systems are affected.
  • Star: This approach is essentially a collection of point-to-point integrations. In a star configuration, every application might connect directly to several other applications. This offers high functionality and flexibility as each integration is independent. However, as your number of connected applications grows, managing and maintaining all those individual connections can become increasingly complex.
  • Enterprise service bus (ESB): This is often considered the most sophisticated integration strategy, typically used in larger organizations. An ESB acts as a central communication system that links all your applications. The key difference from "hub and spoke" is that applications connect to the ESB, but not directly to each other. When data changes, the ESB acts like a data delivery service, routing messages to all applications that need that information. This makes it incredibly flexible for adding or removing applications without disrupting the entire ecosystem.

Pushing and pulling data

Regardless of the integration type you choose, the data itself needs to be exchanged between systems. This typically happens in one or two ways:

  • Pulling (or polling): In this method, the integrating system actively "asks" the source application for new or updated data at regular intervals. It's like checking your mailbox every hour to see if new mail has arrived. The integration makes an API request on a defined frequency (for example, daily or hourly) looking for changes. 
  • Pushing: Here, the source application automatically "sends" data to the integrating system as soon as a change or new record occurs. This is more like getting a text message notification when new mail arrives. The application being integrated sends a notification upon creation or update of records, often using mechanisms like webhooks or a publisher/subscriber model.

This real‑time exchange is especially important when organizations are trying to act on insights quickly, rather than relying on outdated reports or manual checks.

Unlocking seamless operations

Navigating the world of software integration doesn't have to be daunting. By understanding these fundamental concepts, from the role of APIs to the different architectural patterns and data exchange methods, you're now equipped to approach integration discussions with clarity and confidence.

The right integration strategy enables efficiencies that create a more resilient operational environment in the long term. These same foundations are what support advanced analytics and AI to deliver meaningful, trusted outcomes because systems, data and workflows are already connected.

There’s no one-size-fits-all solution; the best approach will always align with your specific organizational needs, existing infrastructure and strategic goals. But by understanding how integrations are built, how data moves between systems and how changes propagate across your ecosystem, you can design connections that scale with your needs and support long‑term operational success.

Discover how continuous, high-quality data fuels smarter decisions and real operational impact with our overview, Defining the AI flywheel: Your blueprint for successful AI integration.

FAQs about software integration

What exactly is software integration?

A software integration is the process of connecting two or more separate software applications so they can communicate, share data and work together seamlessly. This helps to automate processes, reduce manual effort and ensure information flows freely across different systems.

Why are APIs so important for integration?

APIs (Application Programming Interfaces) are crucial because they provide a standardized way for different software applications to interact. They act like a common language and a set of rules that allow applications to request information, send commands or exchange data with each other, much like a universal remote control for your software.

Why is software integration important for analytics and AI?

Analytics and AI depend on complete, up-to-date and consistent data. When data is fragmented across systems, insights become unreliable. Software integration connects those systems, creating a shared foundation that allows analytics and AI to operate in an accurate, trustworthy context.

When should I use a point-to-point integration versus an ESB?

Point-to-point integrations are best for simple scenarios where you only need to connect two applications directly. They're quick to implement but can become complex and hard to manage as the number of connections grows.

An enterprise service bus (ESB) is ideal for larger, more complex environments with many applications. It provides a central, flexible system for all applications to communicate through, making it easier to add or remove systems without disrupting others.

Are APIs enough to support AI-driven decision-making?

APIs enable applications to communicate, but they don’t manage how data flows, changes or stays synchronized over time. Integration platforms and architectures ensure data is orchestrated reliably across systems, which is essential for analytics and AI to deliver meaningful results.

How does integration reduce friction for teams using data and AI tools?

Integrated systems reduce manual data entry, duplicate records and outdated reporting. This gives teams faster access to reliable information, increases confidence in insights and makes it easier to act on recommendations without second-guessing the data behind them.

Do I need an integration platform if I have APIs?

Yes, typically. While an API provides the interface for communication, an integration platform (like Microsoft Azure Logic, Mulesoft or AWS) is the tool that orchestrates and manages the communication flow between different APIs. It handles the logic, scheduling and error handling, making the integration robust and scalable.

Get insights from us

Get Quarterly Insights