Blog

Understanding mean time between failures (MTBF) in the context of CMMS software and enterprise asset management

The concept of mean time between failures (MTBF) is a critical metric in the realms of maintenance, reliability engineering and asset management. It serves as a cornerstone for industries reliant on the continuous and efficient operation of machinery and equipment, particularly in the manufacturing sector. In this article, we delve into the essence of MTBF, its relationship with computerized maintenance management software (CMMS), and enterprise asset management (EAM), highlighting its paramount importance in the manufacturing industry with real-life examples. 

What is mean time between failures (MTBF)? 

Mean time between failures (MTBF) is a reliability metric used to predict the time elapsed between inherent failures of a system or component during its operational phase. It is essentially a measure of how reliably a product, component or system performs over time, expressed typically in hours. The higher the MTBF, the more reliable the equipment is considered to be. MTBF is crucial for planning maintenance, improving product designs and helping ensure the reliability of equipment. 

How can MTBF be used to predict future failures?

Mean time between failures (MTBF) can be used to predict future failures to some extent. MTBF provides an estimate of the average time between inherent failures of a system or component during normal operation. By analyzing historical MTBF data, organizations can make predictions about the reliability and availability of their assets going forward.

Using MTBF for predictive maintenance

MTBF data can be leveraged for predictive maintenance scheduling. By understanding the average time between failures, maintenance teams can proactively plan preventive maintenance activities before expected failure points occur. This helps minimize unexpected downtimes and helps ensure maintenance is conducted during planned production halts, reducing the impact on manufacturing output.

Limitations of MTBF for failure prediction

However, it's important to note that MTBF has some limitations when it comes to predicting future failures:

  • MTBF assumes a constant failure rate, which may not always be accurate, especially for components with wearing parts that increase the chance of failure over time.
  • MTBF is an average, so individual components may fail much earlier or later than the calculated MTBF. It doesn't provide a precise prediction for any specific asset.
  • MTBF does not account for external factors that can influence failure rates, such as operating conditions, age and maintenance practices.
  • Accurately calculating MTBF requires consistent data collection on failures and operating time. Inconsistencies in data can skew the MTBF calculation.

To overcome these limitations, MTBF should be used in conjunction with other reliability metrics, condition monitoring data and maintenance strategies to gain a more comprehensive view of asset health and make informed predictions about future failures. Regular review and updating of MTBF calculations based on new data can also improve the accuracy of predictions over time.

How accurate is MTBF in predicting future failures?

Probability distribution of failures

Using the exponential distribution for reliability calculation, the MTBF represents the time by which 63% of the equipment has failed. This means only 37% of equipment remain operational by the time they reach their MTBF. Mistaking MTBF as the minimum expected time between failures can lead to disappointment, as 63% of equipment have already failed by then.

Comparing MTBF predictions

Comparing MTBF calculations using different assumptions can lead to considerable differences in prediction. Comparing MTBF based on one set of assumptions with an alternative calculation based on different assumptions is meaningless. Using the same base assumptions to compare components or designs is more helpful.

Alternatives to MTBF

To overcome the limitations of MTBF, reliability physics analysis (RPA) is sometimes used instead. RPA directly accounts for global assembly effects, detailed housing geometry, board layout, fixturing and more, enabling evaluation of reliability as the design matures.

How do different reliability prediction standards impact MTBF accuracy?

Different reliability prediction standards significantly impact the accuracy of mean time between failures (MTBF) calculations by influencing the methodologies and assumptions used in determining failure rates. Here are some key points regarding how these standards affect MTBF accuracy.

Variety of standards

There are several established reliability prediction standards, such as MIL-HDBK-217, Telcordia SR-332, 217Plus and others. Each standard employs distinct equations and methodologies to compute failure rates for various components, which can lead to different MTBF outcomes depending on the chosen standard.

Assumptions and methodologies

Each standard has its own set of assumptions regarding failure rates, operating conditions and environmental factors. For example, some standards may assume a constant failure rate during the useful life of a product, while others might incorporate adjustments based on environmental severity or component stress levels. This variability can lead to significant differences in the predicted MTBF.

Adjustment factors

Many standards allow for the incorporation of adjustment factors based on empirical data or specific conditions. For instance, the Telcordia standard includes methods to adjust failure rates based on lab or field data, which can refine predictions to better reflect actual performance. The ability to modify predictions based on real-world data enhances the accuracy of MTBF calculations.

Comparative usefulness

While MTBF predictions can vary widely between standards, they are often most useful for comparative purposes. Using the same assumptions across different components or designs allows for meaningful comparisons, but switching between standards without maintaining consistent assumptions can lead to misleading conclusions.

MTBF and its relevance to CMMS software 

Computerized maintenance management system (CMMS) software is a digital tool that helps organizations manage their maintenance operations more effectively. It includes functionalities for scheduling maintenance, managing inventory, tracking work orders and analyzing maintenance data. The integration of MTBF data into CMMS software enables:

  • Predictive maintenance scheduling: By understanding the average time between failures, maintenance teams can schedule preventive maintenance activities proactively to avoid unexpected downtimes. 

  • Resource optimization: MTBF data helps in prioritizing maintenance tasks based on the criticality and reliability of assets, supporting optimal allocation of resources. 

  • Performance analysis: CMMS software can analyze historical MTBF data to identify trends, evaluate the effectiveness of maintenance strategies and make informed decisions to improve asset reliability. 

Enterprise asset management (EAM) and MTBF 

Enterprise asset management (EAM) encompasses a broader scope than CMMS, focusing on the optimal lifecycle management of an organization's physical assets. EAM involves strategic planning to maximize asset utilization, improve quality and enhance asset-related decision-making. MTBF is integral to EAM as it provides: 

  • Lifecycle cost analysis: Incorporating MTBF data allows organizations to assess the total cost of ownership (TCO) of assets, balancing maintenance costs against the cost of asset failure. 

  • Asset reliability and risk management: MTBF data aids in identifying reliability issues and potential risks associated with asset failure, enabling organizations to implement risk mitigation strategies. 

  • Performance benchmarking: By benchmarking MTBF against industry standards, organizations can gauge their performance and identify areas for improvement in asset management practices. 

Importance in the manufacturing industry 

In the manufacturing industry, where production lines and machinery are the backbones of operational efficiency, MTBF takes on a critical role. A high MTBF indicates reliable machinery, leading to: 

  • Reduced downtime: By minimizing unexpected failures, manufacturing plants can ensure continuous production, leading to higher productivity and profitability. 

  • Quality assurance: Reliable equipment maintains consistent quality in production processes, reducing the likelihood of defects and rework. 

  • Cost savings: Proactive maintenance based on MTBF data can significantly reduce repair costs and extend the lifespan of machinery. 

MTBF in automotive manufacturing use case

An automotive manufacturing plant relies heavily on its assembly line machinery, robotics and other critical equipment to maintain high production rates and help ensure product quality. Unplanned downtime due to equipment failure can lead to significant financial losses, production delays and a negative impact on the supply chain. 

Application of MTBF

The plant management decides to implement a strategic maintenance program focused on maximizing the mean time between failures (MTBF) of their critical machinery. By analyzing historical failure data, the team identifies patterns and the average lifespan of various components within their assembly line equipment. 

Benefits

  • Predictive maintenance: Utilizing MTBF data, the plant schedules predictive maintenance activities before expected failure points, minimizing unexpected downtime. This approach allows for maintenance to be conducted during planned production halts, reducing the impact on manufacturing output. 

  • Resource optimization: With a clearer understanding of equipment reliability, the plant can prioritize maintenance resources toward machinery with lower MTBF values, helping ensure high-value assets receive the attention needed to prevent costly breakdowns. 

  • Improved equipment purchasing decisions: The MTBF data informs future purchasing decisions, guiding the company toward investing in machinery and components known for longer lifespans and reliability, further enhancing production efficiency. 

  • Cost reduction: Proactive maintenance and improved equipment reliability lead to lower repair costs, fewer production stoppages and reduced waste from defective products, directly contributing to the bottom line. 

MTBF in food and beverage use case

In the food and beverage industry, production facilities must manage a variety of equipment such as mixers, conveyors and refrigeration units. The failure of any key component can disrupt production lines, lead to food spoilage and affect compliance with safety standards, resulting in financial loss and damage to the brand's reputation. 

Application of MTBF

A food processing company integrates MTBF analysis into their maintenance management system, focusing on critical equipment that impacts production continuity and food safety. The analysis includes evaluating historical data on equipment failures and identifying trends related to specific types of machinery. 

Benefits

  • Enhanced food safety: By helping ensure equipment operates reliably through MTBF-guided maintenance, the company minimizes the risk of contamination and spoilage, upholding food safety standards and consumer trust. 

  • Production efficiency: Scheduled maintenance based on MTBF data helps maintain the efficiency of production lines, helping ensure that products are produced and delivered on time, meeting market demand without interruption. 

  • Energy efficiency: Regular maintenance of refrigeration units and other energy-intensive equipment, guided by MTBF data, helps these systems operate at peak efficiency, reducing energy consumption and lowering operational costs. 

  • Inventory management: Understanding the expected lifespan of equipment components allows for better inventory management of spare parts, helping ensure that critical replacements are on hand when needed, without overstocking. 

Mean time between failures (MTBF) is more than just a metric; it's a vital tool for predictive maintenance, strategic planning and supporting the reliability and efficiency of equipment in the manufacturing sector. Through the integration of MTBF data into CMMS software and EAM solutions, organizations can achieve optimal asset performance, reduce operational risks and maintain a competitive edge in the market. Real-life examples across various industries underscore the transformative impact of MTBF on maintenance strategies, underscoring its significance in the quest for operational excellence. 

How does MTBF differ from MTTR?

Mean time between failures (MTBF) and mean time to repair (MTTR) are both critical metrics used in maintenance and reliability engineering, but they serve different purposes and provide distinct insights into equipment performance.

Definitions

  • MTBF: This metric measures the average time between failures of a repairable system during its operational life. It indicates how long equipment can function before experiencing a failure. A higher MTBF signifies greater reliability and availability of the equipment.
  • MTTR: This metric measures the average time required to repair a system after a failure has occurred. It includes the time taken to diagnose the issue, perform the repair and bring the system back to operational status. A lower MTTR indicates more efficient repair processes.

Key differences

Focus

  • MTBF focuses on the reliability and uptime of equipment, reflecting how long it can operate before failing.
  • MTTR focuses on the efficiency of the repair process, indicating how quickly a system can be restored to service after a failure.

Application

  • MTBF is used to assess the reliability of equipment and to inform maintenance planning and scheduling. It helps organizations understand how often failures are expected to occur.
  • MTTR is used to evaluate the effectiveness of maintenance operations. It helps identify areas for improvement in repair processes and can inform strategies to reduce downtime.

Impact on operations

  • A high MTBF indicates that equipment is reliable, leading to less frequent disruptions in operations.
  • A low MTTR indicates that when failures do occur, they can be addressed quickly, minimizing the impact on overall productivity.

While both MTBF and MTTR are essential for understanding equipment performance, they provide different insights. MTBF helps organizations gauge reliability and plan for maintenance, while MTTR focuses on the efficiency of repair processes. Together, they offer a comprehensive view of operational effectiveness, enabling organizations to optimize both uptime and maintenance strategies.

How can MTBF and MTTR be used together to predict downtime?

Mean time between failures (MTBF) and mean time to repair (MTTR) can be used together to predict downtime effectively. By combining these two metrics, organizations can gain insights into both the reliability of their systems and the efficiency of their repair processes, allowing for better planning and management of operational downtime.

Understanding availability

  • MTBF measures the average time between failures, indicating how long a system operates before it fails. A higher MTBF suggests greater reliability.
  • MTTR measures the average time required to repair a system after a failure occurs. A lower MTTR indicates a more efficient repair process.

Assessing performance

By analyzing MTBF and MTTR together, organizations can assess their overall performance and identify areas for improvement. If expected downtime exceeds acceptable limits, efforts can be made to increase MTBF (for example, through better maintenance practices) or reduce MTTR (for example, by improving repair processes).

Using MTBF and MTTR in conjunction allows organizations to create a more comprehensive strategy for managing downtime. By understanding the relationship between these metrics, businesses can optimize their maintenance strategies, improve system reliability and enhance overall operational efficiency.

Get insights from us

Get Quarterly Insights