Blog

How asset data insights can drive the shift from reactive to predictive maintenance

Key Takeaways

  • Asset intelligence helps close the gap between asset condition and maintenance response by combining sensor data with EAM and CMMS systems, enabling teams to identify issues early before they result in costly failures.
  • Predictive maintenance uses AI and machine learning to analyze real-time and historical asset data, helping organizations reduce unplanned downtime, eliminate unnecessary maintenance, and make more effective use of maintenance budgets.
  • Integrating maintenance systems and smart data preserves valuable institutional knowledge and builds confidence in data-driven decision-making, enabling organizations to move from reactive and scheduled maintenance toward predictive and eventually prescriptive maintenance strategies.

Despite swimming in data, asset intensive organizations remain trapped in reactive maintenance cycles, unaware of what their assets are telling them.

Subtle warning signs, such as minor shifts in vibration, temperature or voltage, often signal serious underlying issues. Left untreated, these issues can trigger costly downtime, missed deadlines and severe safety risks.

Yet with little visibility into real-time asset health, many organizations still rely on the same approaches used for decades: scheduled or reactive maintenance.

The operational disconnect

Traditionally, maintenance programs have suffered from a major operational disconnect. While asset infrastructure and industrial machinery generate enormous volumes of data every day, much of this information remains isolated within sensors and operational systems.

At the same time, Enterprise Asset Management (EAM) and Computerized Maintenance Management Systems (CMMS) house critical asset information used for lifecycle and maintenance planning. However, many still rely on people manually inspecting and identifying issues before a work order is triggered.

The result is a blind spot between actual asset condition and operational response. This is compounded by the fact that time-based maintenance tends to be uniform, while overlooking differences in workloads, environmental conditions or degradation patterns. It can also be highly resource-intensive, with up to 40% of maintenance budgets spent on unnecessary servicing and production costs.

While the reactive, "fix it when it breaks" approach avoids all that upfront investment, the financial risks of emergency fixes are steep: three to five times more than planned or predictive lifecycle interventions, according to the IPWEA International Infrastructure Management Manual (IIMM).

Building asset intelligence

Many organizations already possess the data they need to move beyond reactive or routine maintenance. It simply is not working hard enough for them.

Predictive maintenance utilizing machine learning AI, the next step in maintenance maturity, addresses this by building asset intelligence through the integration of sensor data with EAM and CMMS.

Siemens asset management solutions like Assetic, Confirm and Asset Essentials establish a foundational layer for asset intelligence, managing data for routine maintenance and lifecycle planning. Building on this, Senseye Predictive Maintenance utilizes intelligent sensors and real-time condition monitoring, using an organization's own data to predict potential issues by identifying subtle deviations in behavior, thereby continuously enhancing asset management and minimizing manual data handling.

By analyzing real-time performance alongside historical data, machine-learning models can identify emerging issues and suggest potential causes based on previous events, helping manufacturers reduce unplanned machine downtime by up to 30%.

Knowledge capture

Besides supporting decision-making in high-stakes environments, another powerful benefit of integrating maintenance systems and data is knowledge capture.

Veteran engineers and technicians often possess decades of knowledge about asset behaviors, recurring faults and successful interventions. When these people leave, much of that knowledge leaves with them — a growing challenge as organizations navigate an aging workforce.

By integrating Siemens EAM with Senseye, asset service levels, maintenance histories and real-time condition data become part of a shared intelligence ecosystem. This dramatically accelerates learning for less experienced workers by preserving the knowledge of how experienced employees have solved previous problems.

Building confidence in prediction

The ultimate destination is prescriptive maintenance, where AI-driven recommendations help teams determine when maintenance is most appropriate. In this environment, operators can see scheduled maintenance approaching, and while adhering to statutory and safety requirements, can consider deferring or skipping it based on actual asset performance and condition.

Reaching this point takes time and trust. However, the opportunity is substantial.

BlueScope Steel, for example, has used real-time data and early warnings from Senseye to shift from reactive maintenance toward a proactive, data-driven approach — preventing approximately 2,000 hours of downtime and 53 process stops globally.

After four years of monitoring thousands of assets and building confidence in the system, BlueScope was able to move away from scheduled servicing and perform maintenance based on predictive insights generated by the platform.

Putting data to work

Australia's infrastructure challenge is immense. With billions of dollars in aging assets requiring renewal, replacement is simply not always an option. Infrastructure must adapt by becoming smarter.

Together, Siemens asset management and predictive maintenance capabilities can help organizations connect asset condition with maintenance planning, make better use of existing data and move progressively from reactive toward proactive maintenance.

To learn more about how Siemens’ asset management solutions integrate with Senseye, or to book a demo, talk to one of our experts today.

 

References:

Siemens AG. (2024). The True Cost of Downtime: Mastering data management and AI-driven machine health. Siemens Digital Industries.

Australian Local Government Association. (2026). National state of the assets report.

 

Get insights from us

Get Quarterly Insights