Blog

CMMS is not enough: Why hospitals need full asset lifecycle visibility

Key takeaways

  • CMMS provides essential operational visibility, but on its own, it leaves hospitals exposed to unmanaged asset risk and underinformed capital decisions.
  • Aging infrastructure, deferred maintenance and limited condition insight are increasing reliance on reactive repairs and straining already constrained capital budgets.
  • Connecting maintenance, risk and capital planning data through an asset lifecycle approach is critical to reducing risk, justifying investment and protecting long-term care delivery.

For many hospitals, implementing a computerized maintenance management system (CMMS) is a critical first step toward improving maintenance operations. But tracking work orders alone isn’t enough to manage today’s complex healthcare environments. With aging infrastructure, rising costs and increasing compliance demands, hospitals need a more comprehensive, data-driven approach.

Leading organizations are moving beyond CMMS to gain full asset lifecycle visibility, connecting maintenance data with capital planning, risk insights and long-term strategy.  

The limits of CMMS alone

At a time when healthcare facilities are facing numerous challenges to improve operations with tighter budgets while maintaining high-quality patient and community care, organizations are also tasked with addressing wider facilities mandates, including meeting sustainability metrics, implementing dangerous-weather preparedness and combating cybersecurity threats.

The result is stretched facilities teams that often fall into costly reactive and deferred maintenance routines that can directly impact patient outcomes.

Recent Siemens Asset Management tracking data suggests that deferred maintenance levels in healthcare are trending upward, increasing to approximately 53% nationwide on average.

The domino effect becomes even more stark when we consider that healthcare’s deferred maintenance backlog has reached an estimated cost of $243 billion, with 38% of hospitals reporting that deferred maintenance has directly affected patient care.

For facilities teams, CMMS has become an essential tool for streamlining processes — tracking work orders, managing assets and shifting to preventive maintenance — to keep operations running smoothly.

However, while powerful and useful, a CMMS alone has some notable shortcomings, including limited visibility into asset condition, risk and lifecycle stage. Without this vital data, facilities teams struggle to connect maintenance insights to justify capital planning decisions that can reduce reactive workflow loops. 

The need for full asset lifecycle visibility

In a 2025 State of U.S. Asset & Facilities Management report, 47% of organizations are currently challenged with aging facilities and infrastructure, while only 59% are confident in their ability to predict when assets are likely to fail. These statistics underscore the imperative hospitals now have to manage their assets across the entire lifecycle, from acquisition to replacement.

While a CMMS on its own provides baseline support for the implementation of preventive maintenance to keep assets running, a more robust system is needed to help facilities team with risk mitigation, hitting sustainability targets, producing predictive insights and confidently creating long-term plans for asset health.

When coupled with an asset lifecycle management strategy, a CMMS truly begins to add value by giving asset managers a holistic view of facility operations. This optimization allows the CMMS to act as a central repository of the operational and maintenance data (work orders, repair histories, technician notes, asset downtime, parts used) needed for asset managers to understand and prioritize critical assets — such as HVAC systems, facility power and medical gas — from procurement to replacement.

With asset criticality established, facilities teams can configure the CMMS to perform risk assessments that surface likely failure points as well as the consequences of asset failure. By combining the likelihood and impact of failure, this risk ranking provides data-driven insights for condition monitoring, preventive and predictive maintenance strategies and guides capital planning to justify essential investments.

This integrated approach enables robust benchmarking across facilities and systems. Comparing key performance indicators (KPIs) like mean time between failures (MTBF) or maintenance costs allows hospitals to identify best practices, pinpoint areas for improvement and enable consistent operational excellence.

Connecting data to strategic outcomes

By centralizing actionable maintenance data, an ALM-optimized CMMS also empowers hospital facilities teams to improve collaboration across the operational ecosystem, track deferred maintenance costs and create comprehensive proactive strategies. With this integrated data visibility, facilities teams have the information they need to justify investments, reduce risk and future-proof infrastructure.

The CMMS, when integrated with capital planning tools, enables long-term forecasting and scenario modeling, which support better funding and investment decisions based on real asset condition and performance — moving hospitals from reactive spending to strategic resource allocation for repairs, replacements and upgrades.

Paired with the detailed asset history and risk ranking insights, the CMMS also provides the data needed to implement strategies to mitigate potential failures before they impact patient care or operations, enabling continuous compliance with critical health and safety regulations.

To meet environmental goals, facilities teams can leverage the CMMS sustainability and energy data to identify opportunities to reduce operational costs, optimize resource consumption and drive efficiency initiatives that support better operational performance.

Ultimately, these data-driven insights align facilities management decisions with the hospital’s broader clinical and financial priorities, allowing asset managers to confidently justify their strategies and investments to executive leadership.

Get Quarterly Insights