Case Study

Western Carolina University cuts costs and energy usage with Energy Manager

Cloud-based energy management helped a North Carolina university gain utility visibility and make data-driven decisions about repairs and upgrades 

 Campus buildings nestled in colorful autumn trees and mountainous terrain, highlighting facility management

Western Carolina University

This public university in Cullowhee, North Carolina, has a $5 million utility budget, more than 11,000 students and a campus sprawling over 682 acres.

Brightly Software was acquired by Siemens. All products and services are now offered under the Siemens Asset Management portfolio.

https://www.wcu.edu/

Headquarters
Cullowhee, North Carolina, USA
Products
Industry Sector
Education
We’re at 55% in BTU-per-square-foot reduction, leading the UNC system. But we still need to track it every month.
Reid Conway
Director of Energy and Utilities, Western Carolina University

Gaining visibility into energy usage

Each month, Western Carolina receives a single invoice from Duke Energy that contains charges for all the power used across campus. In the past, Reid Conway, Director of Energy and Utilities, had to blindly trust that the data provided by Duke Energy was accurate. But by using Energy Manager’s Allocations feature, he can now easily identify building energy usage and costs for each individual facility.

The Allocations feature also has allowed Conway to utilize a single Duke Energy bill to distribute usage and cost to 82 subsidiary accounts within Energy Manager. Though the distribution can be based on fixed percentages, meter readings or a combo of both, Brightly Client Services (now a part of Siemens) determined that meter readings were the best fit for Western Carolina University.

With information split by subsidiary accounts, Conway can easily see changes in energy usage compared to historical data to quickly address any problems. 

Tracking usage

Western Carolina University also uses Energy Manager to easily and consistently track the energy used across campus. In recent years, the university has replaced some aging buildings with more efficient facilities and regularly works to update aging infrastructure with more efficient components, reflecting positive trends in usage numbers.

Conway submits an annual university energy usage report to the state energy office, which must include:  

  • Total kilowatt hours of electricity used and the total cost
  • Total therms of natural gas used and the total cost
  • Total gallons of water and the total cost
  • Total facility square feet  

With Energy Manager, it’s easy for Conway to quickly locate totals to complete reports like this — and to celebrate department wins. “We’re at 55% in BTU per square foot reduction, leading the UNC system,” he says. “But we still need to track it every month.”   

Making informed decisions

Conway and his team access the data available through Energy Manager to make informed decisions about facility usage, repairs and updates to help them conserve energy and cut costs. “Being able to compare the energy costs of one building versus another helps us figure out where to put resources,” Conway says.

For example, when special events are held on campus during the summer, Conway can make sure they’re located in the most energy-efficient buildings to use the least energy possible.

In addition, by comparing energy usage among buildings, he can figure out what changes or updates may be needed in less efficient buildings. When the university recently converted an all-electric building to natural gas to conserve energy and cut costs, Conway used Energy Manager to access historical usage data for the building to make sure the natural gas company installed appropriate access to meet the building’s needs. 

Being able to compare the energy costs of one building versus another helps us figure out where to put resources.
Reid Conway
Director of Energy and Utilities, Western Carolina University

Get quarterly insights