Blog

Digital Twins explained: Definition and use cases in asset management

Key takeaways

  • Digital Twins are dynamic virtual replicas that transform asset management from reactive to predictive maintenance and optimized performance.
  • These powerful tools offer numerous practical applications, from enhancing energy efficiency and remote diagnostics to improving lifecycle cost management and compliance reporting.
  • Adopting Digital Twins is an accessible and iterative journey, allowing asset managers to start with available data and progressively unlock greater value as their Digital Twin matures and evolves.

What are Digital Twins?

A Digital Twin is a virtual model of a physical object, system or process that utilizes sensors and real-time data to continuously mirror the behaviors, conditions, materials and performance of its physical counterpart. More than a 3D model, a Digital Twin can run simulations, test scenarios, predict performance, identify potential issues and control its physical twin without touching the asset.

A transformative tool that is leveraged across several industries, Digital Twins allow asset management technicians to maximize the value and longevity of physical assets. By creating a dynamic replica of an asset, Digital Twins help organizations to move from reactive strategies to proactive, predictive maintenance to reduce unexpected downtime and costly emergency repairs — effectively extending asset lifecycles while optimizing maintenance scheduling, resource allocation and operational performance and efficiency.

As organizations look to digitize and automate facility processes, Digital Twins — often used in complex industrial environments — are increasingly being used to replicate healthcare facilities, school campuses, warehouses and retail spaces to simulate asset performance, energy use, occupancy and maintenance strategies.

Here is how Digital Twins work and how facilities teams can implement them to improve asset management.

How do Digital Twins work?

Digital Twins function as dynamic, living models that continuously evolve with their physical counterparts to provide a comprehensive, real-time understanding of an asset’s status and potential lifecycle. They bridge the gap between the physical and digital asset through a continuous feedback loop, enabling proactive decision-making and optimization at every stage of an asset’s life. Here is how that process works:

  • Data gathering and modeling: A comprehensive virtual model of the physical asset mapping its components, behaviors and environment. Real-time data from various sources along the physical asset is ingested to keep the virtual model up to date. Once deployed, real-time sensor data, maintenance logs, historical performance data and environmental conditions are continuously streamed to the Digital Twin.
  • Contextual analysis and simulation: With this rich real-time data stream, the Digital Twin interprets the ingested data within the context of the asset’s design, operational history and environmental factors to predict future behavior, identify anomalies and assess potential risks and failures. For example, by analyzing current vibration data for a critical component against its historical baseline and design specifications, the Digital Twin can predict the likelihood and timing of potential equipment failure weeks in advance.
  • Decision support and action orchestration: Based on its predictions and analyses, the Digital Twin provides actionable insights and can, in some instances, trigger automated actions. It helps asset managers make informed decisions to optimize performance, prevent failures and improve efficiency. Following a prediction of an impending pump failure, for example, the Digital Twin can automatically reroute power to balance load and prevent outages during peak demand.
  • Continuous learning and refinement: Digital Twins learn from every interaction, prediction and outcome. The feedback from real-world actions taken from their insights refines their models, algorithms and predictive capabilities, making it increasingly accurate and valuable over time. This continuous learning helps the Digital Twin remain an effective tool for managing assets from initial integration to decommissioning.

By integrating these capabilities, Digital Twins transform asset management from a reactive, costly practice into a proactive, value-generating strategy. They give organizations the tools and information needed to achieve higher uptime, lower operational costs, extend asset life and make smarter, data-driven decisions across their entire asset portfolio.

Eight practical Digital Twins use cases in asset management

Digital Twins are helping organizations transform their asset management strategies, allowing them to move from costly reactive maintenance processes to proactive, predictive maintenance cadences that offer significant cost saving across the entire asset lifecycle.

Here are some of the most impactful applications emerging in asset management environments.

Predictive maintenance and anomaly detection

The Digital Twin continuously monitors real-time sensor data from physical assets, including temperature, vibration, pressure, energy use and more. By comparing this data against historical performance, design specifications, and operational norms, the twin can detect subtle anomalies or deviations that signal potential issues. This allows maintenance teams to proactively schedule interventions, minimizing unplanned downtime and extending asset lifespan.

Performance optimization and energy efficiency

The Digital Twin simulates various operational scenarios and analyzes real-time performance data to identify inefficiencies. It can model the impact of different settings, loads, and environmental conditions on asset performance and energy consumption. Asset managers can use these insights to fine-tune operating parameters for maximum output, reduced energy use or extend component life.

Remote monitoring and diagnostics

Digital Twins provide a comprehensive, real-time view of asset health and status from anywhere. Asset managers and technicians can remotely access the twin to diagnose issues, review performance trends and understand the context of an alert without being physically present at the asset’s location. This reduces travel time and costs for diagnostic visits, speeds up problem resolution and enables maintenance teams to support assets globally.

Lifecycle cost management and investment planning

The Digital Twin aggregates data on asset acquisition costs, operational expenses, repair histories and projected remaining useful life. It can simulate the financial implications of different maintenance strategies, upgrades or replacement schedules. For asset managers, this helps provides the data-driven insights to optimize and support capital and investment decisions, including when to repair, refurbish or replace assets to maximize return on investment. 

Compliance and regulatory reporting

Acting as a central repository for all asset-related data, the Digital Twin can automatically generate reports based on maintenance, records, inspection reports, operational parameters and environmental performance. Asset managers can leverage reports to create the documentation required for regulatory compliance. By simplifying auditing process, the Digital Twin enables adherence to safety and environmental standards as well as reduce administrative burden and potential penalties.

Training and onboarding simulation

As an interactive tool, Digital Twin environments can serve as realistic training grounds for new technicians to practice procedures, troubleshoot simulated faults and familiarize themselves with complex systems in a safe, virtual space. This reduces the risk of errors on live equipment, accelerates skill development and provides a consistent, high-quality training experience.

Scenario planning and risk assessment

Digital Twins can simulate the impact of various external factors — extreme weather, supply chain disruptions, increased demand — or internal changes such as component failure and operational changes on an asset or an entire system. This enables asset managers to proactively assess risks, develop contingency plans and understand the potential consequences of different decisions before implementing them across the physical asset landscape.

AI-enhanced Digital Twins for autonomous operations

When integrated with AI and learning, Digital Twins deeply analyze extensive data streams. This allows asset managers to surface complex insights, leading to automated decision-making or informed recommendations that can be applied to the physical asset.

As Digital Twins become integral to asset management, their true value emerges in improved maintenance and operations by serving as the bridge between day-to-day asset performance and broader organizational goals. This growing role lays the foundation for a more coordinated, data-driven operational environment.

Embracing Digital Twins in asset management ecosystems

Often thought of as a tool for highly-specialized and industrial sectors, Digitals Twins can also be indispensable in asset lifecycle management, where organizations are navigating increasingly complex operational environments — helping asset managers to better digitize and automate their work flows and processes.

Key for asset managers looking to adopt Digital Twins into their toolkit is the understanding that a perfect, fully autonomous system is not needed to start. The iterative nature of the technology means that they can be employed using basic data to build a simple connection between the physical asset to the virtual one, to more sophisticated models paired with AI for autonomous operations.

This evolution is further supported by initiatives like the ISO 19650 standard, which has enhanced interoperability and cross-sector data sharing in asset management environments. This evolution allows individual Digital Twins to work in concert, unlocking new insights and efficiencies that were previously unattainable when assets were managed in isolation.

The most important takeaway for asset managers is you don’t need perfect data to begin realizing value in using Digital Twins; it simply requires data and a connection between the virtual and physical asset. As data quality improves and the predictive capabilities are continuously refined, the value of Digital Twins also compounds exponentially.

By embracing this dynamic technology, asset managers can achieve unprecedented levels of efficiency, resilience and strategic foresight to help ensure their assets deliver maximum value through their entire lifespan.

Get insights from us

Get Quarterly Insights