Q: Does anyone have an equipment numbering system that they can recommend to me? I'd like to set up a system that will work for the folks in the office as well as the tradesmen, and I'd really like to hear from you if you have a system that works well.
A: Great question. Each piece of equipment will need to have a unique "item number." This item number can be alphanumeric. The best practice is to use a consistent naming convention. How you create them generally depends how you want your equipment displayed in list views and reports. For example, the equipment list view in MaintenanceDirect can be sorted by Item Number or Description. I would recommend you create your item numbers in a way that will group your equipment either by location or types of equipment.
It is ideal for the item number to be easily recognizable and you can identify exactly what the equipment is by looking at the item number. Here is an example of how we might see item number commonly used:
JHS-AHU-001
JHS-AHU-002
This numbering convention identifies the Location (Jones High School), the type of equipment (Air Handling Unit) and the number of the unit. If you have a number for your location or building code this could also be used. For example:,
120-AHU-001
I hope this helps, and I'm interested in seeing some other client suggestions.
I have also seen a few methods and learned a couple of tricks, especially if you are establishing an ID number.
Many people I've seen will use a series of abbreviations to help look at a list and search for it. The abbreviations often include the site/campus, type of asset and the number. Occasionally, someone may include the trade.
Examples:
ADM_RTU_01 or AdmRTU01
ADM_HV_RTU_01 or AdmHvRtu01
This means it is at the Administration Building and it is a Rooftop Unit that HVAC services. It makes it consistent and easy to search.
Why did I use "_" vs. "-" or "."? Sometimes, certain special characters are treated as wild cards in searches. An underscore usually means something more exact.
Here are some possible acronyms to consider:
Acronym Name
ADO: AUTOMATIC DOOR OPENER
ADU: COMPRESSED AIR DRYER
AED: AUTOMATIC EMERGENCY DEFIBRILLATOR
AFD: AUTOMATIC FIRE DETECTION - SMOKE DETECTOR
AHU: AIR HANDLER UNIT
AMP: AMP THEATER
ARD: AIR DOOR
BBG: BASKETBALL GOALS
BFL: BACKFLOW PREVENTER
BLR: STEAM BOILER
BLR: BOILER
BPS: BACK-UP POWER SUPPLY
BPS: BATTERY POWER SYSTEM
BRE: BREAKER
BRK: BREAKER, CIRCUIT
BRL: BROILER
BRZ: BRAZER, TILT
CDR: CONDENSER
CIRC: CIRCULATOR PUMP
CLR: CHLORINATION SYSTEM POOL
CMP: COMPRESSOR
CTR: CONTROLLER
CTS: CHEMICAL TREATMENT SYSTEM
DMP: DAMPENER
DRY: CLOTHES DRYER
DSD: DUCT SMOKE DETECTOR
DSP: DISPOSAL
DST: DUST COLLECTER
DWR: DISHWASHER
EC: EVAPORATIVE COOLER
ECO: ELECTRICAL CONTROL
EDP: ELECTRICAL DISTRIBUTION PANEL
EEW: EMERGENCY EYE WASH
EF: EXHAUST FAN
ELV: ELEVATOR
EML: EMERGENCY LIGHTING
EMS: EMERGENCY WASH
EVP: EVAPORATOR COIL
EVP: EVAPORATOR
FAN: FAN ALL
FB: FIRE BLANKET
FCO: FIRE CONTROL OPERATORS
FD: FIRE DOOR
FDR: FIRE DOOR ROLLUP
FFI: FIRE FLOW INDICATOR
FFV: FIRE FLOW VALVE
FH: FIRE HOSE
FHC: FIRE HOSE CONNECTION
FIL: POOL FILTRATION
FIS: FIRE SUPPRESSION SYSTEM
FRY: FRYER, DEEP
FWM: FOOD WARMER
FXT: FIRE EXTINGUISHER
FZR: FREEZER
GAS: GAS UTILITIES
GND: GRINDER
GTE: GATE
HOD: HOOD, EXHAUST, KITCHEN
HTB: HOT TABLE
HTR: HEATER
ICE: ICE MACHINE
KET: KETTLE
LFT: LIFT POOL
LPD: L.P. GAS DETECTOR
MCC: MOTOR CONTROL CENTER
MTR: MOTOR
MXR: MIXER
OVN: OVEN
PGS: PLAYGROUND STRUCTURE
PRH: PERIMETER HEATING
PSC: PRESSURE COOKER
PWS: POWER SOURCE
REF: REFRIGERATOR
REG: REGULATOR, PRESSURE
RNG: RANGE TOP
RTB: REFRIGERATED TABLE
RTU: ROOFTOP UNIT (AIR HANDLING UNIT)
SBP: SWITCHBOARD PANEL
SLP: SOLAR PANEL
SLR: SLICER
SRV: SERVER
STM: STEAMER
SWB: SWITCHBOARD
SWG: SWITCHGEAR
SWH: SWITCH HIGH VOLTAGE
SWS: SWITCH SAFETY
TMR: TIMER
TNKP: TANK PRESSURIZED
TRF: TRANSFORMER
VAL: VALVE
VAV: VARIABLE AIR VOLUME BOX
VFD: VARIABLE FREQUENCY DRIVES
WAS: CLOTHES WASHER
WC: WATER COOLER
WCL: WHEELCHAIR LIFT
WH: WATER HEATER
WIC: WALK-IN COOLER
WIF: WALK-IN FREEZER
WS: WATER SOFTENER